Keysight VISA.NET Help
WriteLineList(Single[]) Method



The array of singles to be added to the formatted I/O write buffer.
Converts each of the singles in the specified array to an ASCII string and appends them, separated by commas, to the formatted I/O write buffer. Appends a newline (0xA) to the formatted I/O write buffer, flushes the buffer, and sends an END with the buffer if required.
Syntax
'Declaration
 
Overloads Sub WriteLineList( _
   ByVal data() As Single _
) 
'Usage
 
Dim instance As IMessageBasedFormattedIO
Dim data() As Single
 
instance.WriteLineList(data)
void WriteLineList( 
   float[] data
)
void WriteLineList( 
   array<float>^ data
) 

Parameters

data
The array of singles to be added to the formatted I/O write buffer.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025